MMT area editor bug?
- September 25, 2025
- 2 replies
- 369 views
I have problems with using Memory Management Tool (MMT) in CubeMX v6.15.0 and CubeIDE is v1.19.0. MCU is STM32H7R3L8H6H.
Here's the MMT view and DTCM area of Boot in focus:
As you can see, DTCM area is 64 KB.

But in CORTEX_M7_BOOT MPU peripheral view it is 128 MB:

Same thing goes into Boot\Core\Src\main.c function MPU_Config:
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0x20000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_128MB;
MPU_InitStruct.SubRegionDisable = 0xEE;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);But this next thing is complete nonsense. Here's MMT view of external PSRAM area at 0x91E00000:

Generated MPU config code is:
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER6;
MPU_InitStruct.BaseAddress = 0x91E00000;
MPU_InitStruct.Size = MPU_REGION_SIZE_2MB;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER7;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER8;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);What happens is that same area gets configured 3 times.
I thought its a bug in generator but after checking IOC file I saw this area defined 3 times. I did fiddle around with areas in MMT editor and maybe it broke down and created this mess? I also see wrong DTCM area size in IOC. So maybe it's a bug in MMT editor instead? IOC file is attached.
I have a related question also:
Why is all MPU config done (generated) in boot code? I actually don't want boot to define all the MPU areas because in that case future application releases would be forced to use the setup that boot does. I would prefer if boot configures those areas that are defined in MMT Boot column and App configures those that are in App column.
In MMT wiki I have seen pretty complex pictures when security features are enabled. Maybe some features open up with that? But right now I prefer to keep things simple and do security part later.