Skip to main content
Visitor II
April 9, 2025
Question

Norton finds IDP.Generic threat in stm32cubeide_1.18.0_2441_20250227_1633_x86_64.exe

  • April 9, 2025
  • 1 reply
  • 585 views

On (up-to-date) Windows10-64 machine, I just downloaded and installed (for first time) STM32CubeIDE.  

(Up to date Norton) reports the following "High Threat". Details below.  

The last reference I can find by googling this error goes back to 2020, and was apparently fixed.

Before I click the "make exception" option (or just delete the installer), I want to make sure a true virus hasn't somehow snuck into the current release. 

-bob 

____________________________

Details

Threat name: IDP.Generic
Threat type: Miscellaneous - This is an app that you may have unknowingly installed and that may harm your computer performance.
Status: Threat detected
Detected by: Behavioral Protection
On PC from: 2/27/25, 10:02 AM
Last Used: 4/8/25, 9:33 PM
Startup Item: Yes

Many users
Thousands of users in the Norton Community have used this file.

Mature
This file was released a month ago.

High
The file risk is high.
____________________________

Origin

Location: local://*C:\Users\rober\Downloads\en.st-stm32cubeide_1.18.0_24413_20250227_1633_x86_64.exe\st-stm32cubeide_1.18.0_24413_20250227_1633_x86_64.exe http://zone.identifier.invalid
____________________________

Activity

Path | Type | Status
C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\stm32cubeide.exe | File | Infected
C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\stm32cubeide.exe | Process | Infected

 

 

 

1 reply

Explorer II
August 29, 2025

I'm getting the same with AVG.