Skip to main content
Associate II
September 23, 2025
Solved

Not able to configure mbedtls in STM32CubeIDE

  • September 23, 2025
  • 5 replies
  • 782 views

I want to use the rsa feature of mbedtls but when I uncomment #define MBEDTLS_RSA_C in the mbedtls_config file it is showing undefined reference to mbedtls_rsa_get_len, mbedtls_rsa_check_pub_priv, mbedtls_rsa_init, mbedtls_rsa_free and mbedtls_rsa_import_raw.

 

 

Best answer by Ghofrane GSOURI

Hello @Advait 

I sincerely apologize ,I forgot to mention the steps I have already taken.

In STM32CubeMX, follow these steps to enable RSA support in MbedTLS:

1- Under Middleware, select MbedTLS.
2- Go to the Module tab.
3- Enable the option Show Advanced Parameters.
4- In the search bar, type MBEDTLS_RSA_C.
5- When you find the MBEDTLS_RSA_C option, set it to "Defined" ( select "Defined" from the dropdown).

 

GhofraneGSOURI_0-1759490916679.png

Then Go to Feature support tab and change the value of MBEDTLS_PKCS1_V15 and MBEDTLS_PKCS1_V21 to defined 

GhofraneGSOURI_1-1759491013111.png

Generate and build the code : the rsa.c will be added successfully to your project 

GhofraneGSOURI_2-1759491160699.png

 

I am sorry again 

THX

Ghofrane

5 replies

Ghofrane GSOURI
Technical Moderator
September 24, 2025

Hello @Advait 

Could you please provide your IOC in order to push further the investigation.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
October 1, 2025

Hi @Ghofrane GSOURI 

Sorry for the late reply. Here is my ioc file.

AdvaitAuthor
Associate II
October 1, 2025

Hi @Ghofrane GSOURI 

I accidently logged in with my other account. you can use the ISO file provided above.

Ghofrane GSOURI
Technical Moderator
October 1, 2025

Hello @Advait 

After uncommenting the line #define MBEDTLS_RSA_C, I encountered the following build error:

In file included from ../MBEDTLS/App/mbedtls_config.h:3294,
 from ../Middlewares/Third_Party/mbedTLS/library/camellia.c:31:
../Middlewares/Third_Party/mbedTLS/include/mbedtls/check_config.h:511:2: error: #error "MBEDTLS_RSA_C defined, but none of the PKCS1 versions enabled"
 511 | #error "MBEDTLS_RSA_C defined, but none of the PKCS1 versions enabled"

GhofraneGSOURI_0-1759317100992.png

To resolve this issue, I also uncommented #define MBEDTLS_PKCS1_V21 in the configuration file.
After making this change, the build completed successfully  I did not encounter any undefined reference errors.

GhofraneGSOURI_1-1759317238357.png

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AdvaitAuthor
Associate II
October 3, 2025

Hello @Ghofrane GSOURI 
I uncommented #define MBEDTLS_PKCS1_V21 but its giving this build error.

Advait_0-1759468649389.png

Advait_2-1759469139894.png

 

 

AdvaitAuthor
Associate II
October 3, 2025

I am not able to enable features using the GUI

 

Ghofrane GSOURI
Technical Moderator
October 3, 2025

Hello @Advait 

Are you using the latest version of STM32CubeIDE 1.19.0?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AdvaitAuthor
Associate II
October 3, 2025

No, I am currently on 1.17.0