Skip to main content
Visitor II
August 14, 2024
Solved

NUCLEO-L4R5ZI is not connecting to STM32CubeIde

  • August 14, 2024
  • 1 reply
  • 711 views

Hi,

I have been trying to program NUCLEO-L4R5ZI but the ST-Link doesnt seem to be connecting. I have been going through the forums and it seems the ST-Link drivers dont work with Windows 11. Is that correct?

Thank you.

    Best answer by STTwo-32

    Hello @arbio13 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    The Drivers should work without a problem on Windows11. You may try to:

    • Ensure that you are using a data USB cable and not a charging one.
    • Ensure that you are connecting the board throw the Connector CN1 and not CN14.
    • Follow the guidelines of the UM2179 specially paragraph 3.1.
    • Try using differrent USB ports on the PC.
    • Try to connect the board to Cibe Programmer, upgrade the ST-link version and do a full chip errase. 

    Best Regards.

    STTwo-32 

    1 reply

    STTwo-32
    STTwo-32Best answer
    Technical Moderator
    August 14, 2024

    Hello @arbio13 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    The Drivers should work without a problem on Windows11. You may try to:

    • Ensure that you are using a data USB cable and not a charging one.
    • Ensure that you are connecting the board throw the Connector CN1 and not CN14.
    • Follow the guidelines of the UM2179 specially paragraph 3.1.
    • Try using differrent USB ports on the PC.
    • Try to connect the board to Cibe Programmer, upgrade the ST-link version and do a full chip errase. 

    Best Regards.

    STTwo-32