Skip to main content
Associate II
August 12, 2024
Question

NUCLEO-L4R5ZI-P Printing gibberish on Serial

  • August 12, 2024
  • 2 replies
  • 2990 views

Hello,

 

I just got a NUCLEO-L4R5ZI-P and trying to test it out before i start my project. I tried the simple "Hello!" on serial and displaying via PuTTY cmd on windows. It is printing gibberish or maybe am missing something. Am new to ST and any help will be appreciated. I have tried a number of solutions but same result. Here is the main.c code and the output on PuTTY cmd.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;

UART_HandleTypeDef hlpuart1;
UART_HandleTypeDef huart3;

PCD_HandleTypeDef hpcd_USB_OTG_FS;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_LPUART1_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART3_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */
 uint8_t buf[12];
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_LPUART1_UART_Init();
 MX_USB_OTG_FS_PCD_Init();
 MX_I2C1_Init();
 MX_USART3_UART_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 strcpy((char*)buf, "Hello!\r\n");
	 HAL_UART_Transmit(&hlpuart1, buf, strlen((char*)buf), HAL_MAX_DELAY);
	 HAL_Delay(500);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 2;
 RCC_OscInitStruct.PLL.PLLN = 30;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief I2C1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2C1_Init(void)
{

 /* USER CODE BEGIN I2C1_Init 0 */

 /* USER CODE END I2C1_Init 0 */

 /* USER CODE BEGIN I2C1_Init 1 */

 /* USER CODE END I2C1_Init 1 */
 hi2c1.Instance = I2C1;
 hi2c1.Init.Timing = 0x10A077A8;
 hi2c1.Init.OwnAddress1 = 0;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Analogue filter
 */
 if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Digital filter
 */
 if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C1_Init 2 */

 /* USER CODE END I2C1_Init 2 */

}

/**
 * @brief LPUART1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_LPUART1_UART_Init(void)
{

 /* USER CODE BEGIN LPUART1_Init 0 */

 /* USER CODE END LPUART1_Init 0 */

 /* USER CODE BEGIN LPUART1_Init 1 */

 /* USER CODE END LPUART1_Init 1 */
 hlpuart1.Instance = LPUART1;
 hlpuart1.Init.BaudRate = 115200;
 hlpuart1.Init.WordLength = UART_WORDLENGTH_7B;
 hlpuart1.Init.StopBits = UART_STOPBITS_1;
 hlpuart1.Init.Parity = UART_PARITY_NONE;
 hlpuart1.Init.Mode = UART_MODE_TX_RX;
 hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 hlpuart1.FifoMode = UART_FIFOMODE_DISABLE;
 if (HAL_UART_Init(&hlpuart1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN LPUART1_Init 2 */

 /* USER CODE END LPUART1_Init 2 */

}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 115200;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * @brief USB_OTG_FS Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USB_OTG_FS_PCD_Init(void)
{

 /* USER CODE BEGIN USB_OTG_FS_Init 0 */

 /* USER CODE END USB_OTG_FS_Init 0 */

 /* USER CODE BEGIN USB_OTG_FS_Init 1 */

 /* USER CODE END USB_OTG_FS_Init 1 */
 hpcd_USB_OTG_FS.Instance = USB_OTG_FS;
 hpcd_USB_OTG_FS.Init.dev_endpoints = 6;
 hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL;
 hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
 hpcd_USB_OTG_FS.Init.Sof_enable = ENABLE;
 hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.lpm_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.battery_charging_enable = ENABLE;
 hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE;
 hpcd_USB_OTG_FS.Init.vbus_sensing_enable = ENABLE;
 if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USB_OTG_FS_Init 2 */

 /* USER CODE END USB_OTG_FS_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 HAL_PWREx_EnableVddIO2();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, LD3_Pin|LD2_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : LD3_Pin LD2_Pin */
 GPIO_InitStruct.Pin = LD3_Pin|LD2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : USB_OverCurrent_Pin */
 GPIO_InitStruct.Pin = USB_OverCurrent_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : USB_PowerSwitchOn_Pin */
 GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

PUTTY serial output from STPUTTY serial output from ST

    2 replies

    Andrew Neil
    Super User
    August 12, 2024

    The commonest reason for getting gibberish on a terminal is wrong baud rate:

    https://learn.sparkfun.com/tutorials/serial-communication/all#:~:text=If%20all%20the%20receiving%20device%20sees%20on%20its%20receive%20line%20is%20garbage%2C%20check%20to%20make%20sure%20the%20baud%20rates%20match%20up

    Check your clocking.

    Use an oscilloscope or logic analyser on the wire to see what the actual speed is.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Odd_coderAuthor
    Associate II
    August 21, 2024

    is there another way of checking the baud rate without using the oscilloscope or logic analyzer?

    Associate III
    August 21, 2024

    vishnu_illikkal_0-1724234758157.png

    you can check it in the ioc settings of the uart

    vishnu_illikkal_1-1724234805228.png

    above is the settings that i used in the YAT software on PC
    this settings location may vary with different software
    you must have the same settings on the receiving software / uc as of the ioc settings

    If you are asking about physically finding out the baud rate i haven't done that so I have no idea.

    Associate III
    August 13, 2024

    Try using the software called YAT terminal, this have easy interface, 
    Check whether the setting son both microcontroller and the terminal application are the same
    like Baud rate, Word length, Parity, Stop bits these should be same on both.

    Andrew Neil
    Super User
    August 13, 2024

    @vishnu_illikkal wrote:

    Try using the software called YAT terminal, this have easy interface, 


    Won't make any difference if the baud rate is wrong!

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.