Skip to main content
ASchw.1
Associate II
December 12, 2019
Question

Post build arm-none-eabi-objcopy --gap-fill=0xff in STM32CubeIDE

  • December 12, 2019
  • 3 replies
  • 5102 views

Hello,

I'm using the IDE project properties "MCU Post build outputs" section to enable bin file generation.

0690X00000BuWlAQAV.png

The default behavior though is filling non used gaps in output bin with 0x00, Is it possible to override the "arm-none-eabi-objcopy" with "--gap-fill=0xff" to change default behavior? I couldn't find any place to override this in project properties inside the IDE itself... only run it via post build steps manually and disable the "output bin generation" checkbox above.

Thank you.

3 replies

Ozone
Principal
December 12, 2019

I don't know CubeIDE, but filling gaps (unused space) in actual Flash with 0xFF is common practice.

This avoids Flash wear, and keeps the programming times low.

> The default behavior though is filling non used gaps in output bin with 0x00,

This makes sense for RAM areas, or PC/host-based applications.

danalog
Visitor II
January 21, 2020

I have the same question. I've even set the post-build step command to:

arm-none-eabi-objcopy --verbose -S -O binary --gap-fill 0xFF --pad-to 0x20000 "project.elf" "project.bin"

Set in the STM32CubeIDE project settings as so:

0690X00000BwIIwQAN.png

But my binary is not padded to 128 KB even though it is produced. The only output I receive, despite the --verbose setting, is:

copy from `project.elf' [elf32-littlearm] to `project.bin' [binary]

How can I pad my binary out to the full 128 KB flash size using STM32CubeIDE?

waclawek.jan
Super User
January 21, 2020

Try --pad-to 0x08020000

JW

danalog
Visitor II
January 21, 2020

Perfect, that did work. Thanks JW. I didn't realize the pad-to value is an absolute reference relative to the elf file, not a relative offset.