Skip to main content
Visitor II
November 28, 2025
Question

Problem with StmcubeIDE 2.0.0

  • November 28, 2025
  • 1 reply
  • 211 views

i am getting the below error when running fresh install of stmcubeide 2.0.0 in windows 10. how can i fix this?

"!SESSION 2025-11-27 23:17:13.722 ----------------------------------------------- eclipse.buildId=Version 2.0.0 java.version=21.0.8 java.vendor=Eclipse Adoptium BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US Command-line arguments: -os win32 -ws win32 -arch x86_64 !ENTRY org.eclipse.osgi 4 0 2025-11-27 23:17:16.137 !MESSAGE Application error !STACK 1 java.lang.UnsatisfiedLinkError: Could not load SWT library. Reasons: C:\ST\STM32CubeIDE_2.0.0\STM32CubeIDE\configuration\org.eclipse.osgi\366\0\.cp\swt-win32-4966r5.dll: The specified procedure could not be found no swt-win32 in java.library.path: C:\ST\STM32CubeIDE_2.0.0\STM32CubeIDE;C:\Windows\Sun\Java\bin;C:\Windows\system32;C:\Windows;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility;C:\Users\saeed110\AppData\Local\Microsoft\WindowsApps;C:\Users\saeed110\AppData\Local\Programs\Microsoft VS Code\bin;. no swt in java.library.path: C:\ST\STM32CubeIDE_2.0.0\STM32CubeIDE;C:\Windows\Sun\Java\bin;C:\Windows\system32;C:\Windows;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility;C:\Users\saeed110\AppData\Local\Microsoft\WindowsApps;C:\Users\saeed110\AppData\Local\Programs\Microsoft VS Code\bin;. C:\Users\saeed110\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: The specified procedure could not be found Can't load library: C:\Users\saeed110\.swt\lib\win32\x86_64\swt-win32.dll Can't load library: C:\Users\saeed110\.swt\lib\win32\x86_64\swt.dll C:\Users\saeed110\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: The specified procedure could not be found at org.eclipse.swt.internal.Library.loadLibrary(Library.java:345) at org.eclipse.swt.internal.Library.loadLibrary(Library.java:254) at org.eclipse.swt.internal.C.(C.java:19) at org.eclipse.swt.internal.win32.STARTUPINFO.(STARTUPINFO.java:42) at org.eclipse.swt.widgets.Display.(Display.java:150) at org.eclipse.ui.internal.Workbench.createDisplay(Workbench.java:721) at org.eclipse.ui.PlatformUI.createDisplay(PlatformUI.java:185) at org.eclipse.ui.internal.ide.application.IDEApplication.createDisplay(IDEApplication.java:182) at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:125) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:208) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:143) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:109) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:439) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:271) at java.base/jdk.internal.reflect.DirectMethodHandleAccessor.invoke(DirectMethodHandleAccessor.java:103) at java.base/java.lang.reflect.Method.invoke(Method.java:580) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:668) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:605) at org.eclipse.equinox.launcher.Main.run(Main.java:1481)"

1 reply

Ghofrane GSOURI
Technical Moderator
November 28, 2025

Hello @saeed110 

STM32CubeIDE_2.0.0 is supported on windows 10 .

So let's try the following steps to solve the issue :

1- Uninstall STM32CubeIDE completely.
2- Delete the installation folder (e.g., C:\ST\STM32CubeIDE_2.0.0\).
3- Reinstall the STM32CubeIDE_2.0.0

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.