PWM configuration
Hi, I'm a newbie in this embedded board and I'm having a hard time setting up the PWM pins.
I'm currently using an STM32F103RB with a bldc motor driver shield that has pin 5, 6, 9 for PWM input.
The corresponding pins for them are PB4, PB10, PC7 so I tried to activate pwm for those.
However, PB4(TIM3_CH1) and PC7(TIM3_CH2) couldn't be configured at the same time and when I tried to set PC7 after setting PB4 to TIM3_CH1, PB4 automatically switches to some other pin that can be compatible with PC7.
Why does this happen even if they use the same timer but have different channels?