RE: Cannot connect to STM32 target to erase memory
Hello!
New to the STM controllers, failed to realize that PA13 was necessary to connect the debugger and was quite dismayed to realize my mistake after looking to program it as a GPIO.
I have tried connecting with the IDE and Programmer alike, both with BOOT0 (PA13) to Vdd and without. My latest attempt is shown below which I found another thread about -- even with PA13 shorted to 3.3V and shorted to GND I see the same result -- have I killed my poor STM?
I'm using the NUCLEO-G031J6 while I get accustomed to this microcontroller.
Any advice would be greatly appreciated! Thanks