Skip to main content
Associate II
January 22, 2025
Question

Request for old stm32cubeIDE versions 1.14.0 and 1.15.0

  • January 22, 2025
  • 2 replies
  • 772 views

Hi ST Community,

I am using the board of STM32WBA55CGU6 board for OTA application and i want to use the application present in STM32Cube_FW_WBA_V1.3.0 and STM32Cube_FW_WBA_V1.2.0 packages. Since these packages are present in STM32Cube IDE version 1.15.0 and STM32Cube IDE version 1.14.0 respectively and is not available in the community for installation, i request to send the respective files to the mail id :- " shivaparbati2001@gmail.com "

Thank You.

2 replies

Mike_ST
Technical Moderator
January 22, 2025

Hello,

You can download older WBA packages there:

STM32Cube MCU Package for STM32WBA github 

Select "Tags" instead of "Branches", choose the version and download zip.

 

 

 

ShakuAuthor
Associate II
January 22, 2025

Thank you 

But i have the packages but i want the IDEs (stm32cubeIDE versions 1.14.0 and 1.15.0) as it is not available in ST Community. Please provide the IDEs files.

Peter BENSCH
Technical Moderator
January 22, 2025

@Shaku Newer versions of STM32CubeIDE can work with older firmware versions, but not vice versa. You can and should therefore use the latest STM32CubeIDE and then install the desired firmware version.

Regards
/Peter

ShakuAuthor
Associate II
January 22, 2025

Thank You

After installing the newer version of the IDE the older version's packages are unable to select and unable to use and giving errors regarding errors after compilation.