Set up MPU via CubeIDE to read firmware ID of STM32H563
- September 30, 2024
- 1 reply
- 1617 views
Hi All
I need to access the firmware ID of an STM32H563, while the ICACHE is enabled. As discussed at https://community.st.com/t5/stm32-mcus-products/stm32h563-hard-fault-when-trying-to-read-uid/td-p/584571 this requires setting the memory area as non-cacheable via the Memory Protection Unit.
I'm trying to do this via the ioc configuration in STM32CubeIDE, using a Nucleo-H563ZI board
As the firmware ID is held in a region starting at 0x08FFF800, I expected to set 0x08FFF800 as the MPU region start address (that is what is shown in another user's screenshot on the other post). But the configuration UI says "MPU Region Base Address must be 0x0." and it will not allow any other value to be set.
Could somebody please advise on how I set the 12 bytes starting at 0x08FFF800 as non-cachable ?
Thanks
Nic