Setting up a C++ project for a NUCLEO-F446RE
Apologies for the newbie question, but I am trying to init a project with the following as starting point:
- STM32CubeIDE v1.17.0
- NUCLEO-F446RE
- C++ Development
- FreeRTOS
- CAN Interface
When creating projects it looks like there's a lot of options, but I can't seem to get the combination of C++ and STM32CubeMX file for my NUCLEO board. Two options I've tried for creating a project:
The New "C/C++ Project" with "C++ Managed Build" option:

Produces a `hello-world.cpp` with the following contents:
#include <iostream>
using namespace std;
int main() {
cout << "!!!Hello World!!!" << endl; // prints !!!Hello World!!!
return 0;
}
However it has on specific build target, no STM32CubeMX .ioc file, or ld linker file.
The New "STM32 Project" with "C++" as the "Targeted Language" option:



I get the STM32CubeMX .ioc file for the board but everything otherwise still looks like a C project. All the generated code is in C and the includes don't include anything C++ related.
Edit: Looking at the code closer it seems that maybe this is the structure of the C++ project, however, making a simple class definition it chokes on the the keyword 'class' so I suppose something is still wrong. If someone could steer me towards the right documentation I think that's what I need.
Am I missing something? Also - I'm looking for good STM32CubeIDE tutorials but the 'Tutorial' playlist under STMicroelectronics Youtube channel has no voice over and is sorta useless IMO. So please feel free to direct me to the right materials.
Thanks