Skip to main content
Associate
September 15, 2025
Question

STLINK-V3 not detected by STM32CubeIDE but works with STM32CubeProgrammer

  • September 15, 2025
  • 3 replies
  • 842 views

Hello,

I am experiencing a consistent connection issue with my development setup:

Hardware/Software Configuration:

  • MCU: STM32 (exact model: STM32G474VET6)

  • Debugger: STLINK-V3

  • IDE: STM32CubeIDE

  • Programmer: STM32CubeProgrammer

  • Operating System: Window

  • Target board : Custom board
    • art of custom board schematics : 
      pepsipower_0-1757931591331.pngpepsipower_1-1757931656180.png

Problem Description:

  • When connecting my STLINK-V3 to STM32CubeIDE, the IDE fails to detect or connect to the target device. It typically shows error messages like “No ST-LINK detected” or “No target found.”

  • However, when I use STM32CubeProgrammer, the STLINK-V3 is detected and connects to my target MCU without any issues. All programming and memory read functions work perfectly.

  • While many boards face connection issues with STLINK-V3 in STM32CubeIDE, some boards succeed to be connected.

Questions:

  • Has anyone experienced similar issues where STM32CubeIDE fails but CubeProgrammer succeeds with STLINK-V3?

  • Are there recent changes in CubeIDE or driver packages that could explain this?

  • Any additional steps or patches recommended for resolving this mismatch?

  • Are there any configuration that i can try on CubeIDE? (eg data rate)

3 replies

Andrew Neil
Super User
September 15, 2025

Please show the logs from CubeIDE, and screenshots of the errors.

PS:

Also, what versions, and on what Host?

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
September 15, 2025

Hi,

>  While many boards face connection issues with STLINK-V3 in STM32CubeIDE, some boards succeed to be connected.

The IDE checking the cpu is "genuine STM" , so it refuses connect on all cpus that might be not from STM.

CubeProgrammer connects -if possible- also to other ARM cpus.

But here , on (i assume) genuine STM32G474VET6 , it should connect also in IDE .

Maybe try: set debug to using openOCD  (i had some strange "no target.." , but switching the debug to OCD - it works.  And even switching back the debug setting, it works. This happened also on boards, working before....and then also working again. So dont ask me "why" .)

so try: (and adjust the settings...see:)

AScha3_0-1757936558325.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
September 16, 2025

Thanks all,

I'm out of the office right now. Here i attach the log i get from failure cases....

 

STMicroelectronics ST-LINK GDB server. Version 7.11.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

        Persistent Mode            : Disabled

        Logging Level              : 1

        Listen Port Number         : 61234

        Status Refresh Delay       : 15s

        Verbose Mode               : Disabled

        SWD Debug                  : Enabled

        InitWhile                  : Enabled

 

Target unknown error 19

 

Error in initializing ST-LINK device.

Reason: Unknown. Please check power and cabling to target.


-----

Let me update other properties like host version, Stlink F/W version very soon...