Skip to main content
Visitor II
November 14, 2024
Question

STM32 B-L475E-IOT01A USART1 not working properly transmitting with DMA

  • November 14, 2024
  • 1 reply
  • 561 views

Hello. The USART1 TX works fine when I manually put bytes into the TDR register, but it doesn't work when I try to use DMA in printf function. Below is my initialization and transmitting code (other functions are not shown because they are related to receiving or manual transmitting):

The Transmission Complete interrupt of DMA is never triggered (so next printf call is always waiting for the first one to end), and no message is received by my putty terminal either, while manually sending message works fine.

I've checked my macros for many times according to the programming manual, and I sat here the whole day dealing with it. I worry that it might be damaged because yesterday I put it into the fridge for 5 sec to test the sensor.

Please help :(. I used direct register access to configure DMA because I liked to test my understanding.

 

 

 

#include "stm32l4xx_hal.h"
#include <sys/stat.h>


#define my_BAUDRATE 115200
#define USART_INSTANCE USART1

// GPIO pins
#define my_UART_PC_GPIO_TX_PORT GPIOA
#define my_UART_PC_GPIO_TX_Pin GPIO_PIN_9
#define my_UART_PC_GPIO_RX_PORT GPIOA
#define my_UART_PC_GPIO_RX_Pin GPIO_PIN_10
#define my_UART_PC_GPIO_CLKEN_CMD __HAL_RCC_GPIOA_CLK_ENABLE

// clock enable
#define my_UART_PC_CLKEN_CMD __HAL_RCC_USART1_CLK_ENABLE

// interrupts
#define my_UART_PC_IRQ USART1_IRQn
#define my_UART_PC_IRQ_HANDLER USART1_IRQHandler
#define my_UART_PC_IRQ_PRIORITY 1, 1

// DMA
#define my_DMA_TX DMA1
#define my_DMA_RX DMA1
#define my_DMA_TX_CH DMA1_Channel4
#define my_DMA_RX_CH DMA1_Channel5
#define my_DMA_TX_CHn 4
#define my_DMA_RX_CHn 5
#define my_DMA_TX_IRQn DMA1_Channel4_IRQn
#define my_DMA_TX_IRQHandler DMA1_Channel4_IRQHandler

static void my_NVIC_config();
static void my_clock_config();
static void my_GPIO_config();
static void my_UART_config();

static UART_HandleTypeDef my_UART_handle;
static DMA_HandleTypeDef my_DMA_handle;
uint8_t my_last_recv_byte;
volatile int DMA_TX_busy = 0;
char DMAbuffer[255];

void my_UART_PC_init(){
my_NVIC_config();
my_clock_config();
my_GPIO_config();
my_UART_config();
}

static void my_NVIC_config(){
HAL_NVIC_SetPriority(my_UART_PC_IRQ, my_UART_PC_IRQ_PRIORITY);
HAL_NVIC_EnableIRQ(my_UART_PC_IRQ);
}

static void my_clock_config(){
my_UART_PC_GPIO_CLKEN_CMD();
my_UART_PC_CLKEN_CMD();

__HAL_RCC_USART1_CONFIG(RCC_USART1CLKSOURCE_PCLK2);
}

static void my_GPIO_config(){
GPIO_InitTypeDef GPIO_InitStructure;

// Configure TX pin
GPIO_InitStructure.Pin = my_UART_PC_GPIO_TX_Pin;
 GPIO_InitStructure.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
GPIO_InitStructure.Alternate = GPIO_AF7_USART1;
 HAL_GPIO_Init(my_UART_PC_GPIO_TX_PORT, &GPIO_InitStructure);

// Configure RX pin
GPIO_InitStructure.Pin = my_UART_PC_GPIO_RX_Pin;
GPIO_InitStructure.Mode = GPIO_MODE_AF_PP; // Should be AF for RX
GPIO_InitStructure.Pull = GPIO_NOPULL; // Set the appropriate pull-up/pull-down
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_HIGH; // Speed
GPIO_InitStructure.Alternate = GPIO_AF7_USART1;
HAL_GPIO_Init(my_UART_PC_GPIO_RX_PORT, &GPIO_InitStructure);
}

static void my_UART_config(){
__HAL_RCC_USART1_CLK_ENABLE(); 
__HAL_RCC_DMA1_CLK_ENABLE();

my_UART_handle.Instance = USART_INSTANCE;
my_UART_handle.Init.BaudRate = my_BAUDRATE;
my_UART_handle.Init.WordLength = UART_WORDLENGTH_8B;
my_UART_handle.Init.StopBits = UART_STOPBITS_1;
my_UART_handle.Init.Parity = UART_PARITY_NONE;
my_UART_handle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
my_UART_handle.Init.Mode = UART_MODE_TX_RX;
HAL_UART_Init(&my_UART_handle);

// DMA for TX
my_DMA_TX_CH->CCR &= !DMA_CCR_EN;
USART_INSTANCE->CR3 |= USART_CR3_DMAT; // enable USART DMA
my_DMA_TX_CH->CPAR = (uint32_t) &USART_INSTANCE->TDR; // target address
my_DMA_TX_CH->CMAR = (uint32_t) DMAbuffer;
my_DMA_TX_CH->CCR |= DMA_CCR_MINC | DMA_CCR_DIR| DMA_CCR_TCIE; // memory increment, direction, TXC IRQ
HAL_NVIC_EnableIRQ(my_DMA_TX_IRQn); // enable DMA TX interrupt

__HAL_UART_ENABLE_IT(&my_UART_handle, UART_IT_RXNE);
//__HAL_UART_ENABLE_IT(&my_UART_handle, UART_IT_TXE);
}
int _write(int file, char *ptr, int len) {

 for (int i = 0; i < len; i++) {
my_UART_PC_sendByte((uint8_t)ptr[i]);
 }
 return len; // Return the number of characters written
 
 /*
 while(DMA_TX_busy);
for(int i=0;i<len;i++){
DMAbuffer[i] = ptr[i];
}
 my_DMA_TX_CH->CNDTR=len;
my_DMA_TX_CH->CMAR = (uint32_t) DMAbuffer;
my_DMA_TX_CH->CCR |= DMA_CCR_EN;
DMA_TX_busy = 1;
return len;
*/
}

void my_DMA_TX_IRQHandler(void) {
 // Check for the transfer complete interrupt
 if (my_DMA_TX->ISR & DMA_ISR_TCIF4) {
 my_DMA_TX->IFCR = DMA_IFCR_CTCIF4; // Clear transfer complete flag
 my_DMA_TX_CH->CCR &= ~DMA_CCR_EN; // Disable DMA channel to stop TX
 DMA_TX_busy = 0;
 }
}

 

 

 

 

1 reply

Ghofrane GSOURI
Technical Moderator
November 15, 2024

Hello @ternence 

First let me thank you for posting.

Based on your description and the provided code, here are some potential areas to investigate and suggestions to resolve the problem:

1- Ensure that the DMA is correctly configured before starting the transmission. Specifically, check the following:

  • Enable DMA Clock: Confirm that the DMA clock is enabled before you initialize your UART or start any DMA transfers. The order of initialization is crucial; the DMA must be initialized before it is used by any peripheral.

2- Verify that USART is configured to use DMA for transmission.

3- Check your interrupt handling setup:

  • NVIC Configuration: Ensure that you have configured the NVIC for the DMA channel correctly. The interrupt priority should be appropriate, and it should be enabled.

4- Ensure that your buffer management is correct:

  • Buffer Size: Make sure that DMAbuffer is large enough to hold all data you intend to send. If you're sending more data than it can hold, this could lead to undefined behavior.

5- Consider  using HAL functions like HAL_UART_Transmit_DMA() which abstract away some complexities and might help isolate whether it's a configuration issue or a deeper problem in your setup.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.