Question
STM32CubeIDE failed to import examples on Linux
Hi,
I'm using STM32CubeIDE on latest Ubuntu:
STM32CubeIDE Version: 1.14.1, Build: 20064_20240111_1413 (UTC).
If I try to click "Import STM32Cube example", it shows next window with "target selection" which always fails (can only cancel, no selection possible, see below). Just in case, CubeMX works fine.
Could anyone from ST comment if I miss something or it is a bug on Linux platform?