STM32CUBEIDE: Won't start.
STM32CubeIDE 1.9.0 has been working fine, until tonite. I started it and after it asked which workspace it acted like it was loading but never went anywhere. I killed it, removed the .lock file and restarted and the same thing except it's now exiting. The .ide.log has this:
2022-06-15 23:57:26,297 [INFO] PluginManager:213 - loadIPPluginJar : add gic
2022-06-15 23:57:26,301 [INFO] IPUIPlugin:75 - create IPUIPlugin
2022-06-15 23:57:26,301 [INFO] PluginManager:213 - loadIPPluginJar : add openamp
2022-06-15 23:57:26,624 [FATAL] Updater:297 - Updater called before beeing initialized
2022-06-15 23:57:26,784 [FATAL] Updater:297 - Updater called before beeing initialized
2022-06-15 23:57:26,795 [INFO] DbMcusAds:47 - JSON generation date=Thu Sep 30 02:55:09 EDT 2021 (1632984909247)
2022-06-15 23:57:26,795 [FATAL] Updater:297 - Updater called before beeing initialized
... and it just keeps going. I tried re-installing but it just says "Nothing to install", prolly because it is installed.
OS is Debian whatever the current version is called.
Any ideas on how to get this working again?
Thanks!
Vince.