STM32F746ZGT7 Linker error: "Non-constant or Forward Reference Address Expression"
Dear Support Team,
I am encountering an issue while building my project for the STM32F746ZGT7 in STM32CubeIDE version 1.16.0.And I'm working to "DISPLAY BOARD BRING - UP" During the linking process, I receive the following error message:
Steps to Reproduce:
- Open STM32CubeIDE version 1.16.0.
- Open the STM32F746ZGT7 project.
- Attempt to build the project.
- The error occurs during the linking phase.
Environment:
- STM32CubeIDE Version: 1.16.0
- Toolchain Version: GNU Tools for STM32 (12.3.1)
- Board: STM32F746ZGT7
- Operating System: Windows 10
Description of the Problem:
The error appears to be related to an invalid or forward reference address expression in the linker script STM32F746ZGTX_FLASH.ld at line 184. I have already checked the linker script for any invalid address or section definitions, but the issue persists
Steps Taken to Resolve the Issue:
- I verified the memory regions and configurations in STM32CubeMX, ensuring they are correctly defined.
- I cleaned the project and rebuilt it, but the error still occurs.
Could you kindly provide guidance on how to resolve this issue? Any assistance would be greatly appreciated