Skip to main content
Associate III
October 27, 2025
Question

stm32h7: M7 core resets OK; M4 core stuck in reset handler

  • October 27, 2025
  • 1 reply
  • 209 views

Hi, im using stm32h745bit6 MCU, when im pressing reset button only M7 core is reseting and M4 core is stucking in an reset handler itself, what to do an reset. since if a use system reset also same only.

can u someone suggest what to do for this reset handler issues.

 

 

regards,

srinath

1 reply

mƎALLEm
Technical Moderator
October 27, 2025

Hello,

It's hard to help you based on the description you provided.

What board are you using? What example are you testing?

Please review How to write your question to maximize your chances to find a solution 

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Associate III
October 27, 2025

Hi @mƎALLEm 

stm32h45bit3 208 pin package board we designed, in this normally i have verified peripherals, clocks, etc. during testing when i try to reset the board by push button i can see m7 core resets fine no issues, while m4 core stuck in reset handler.

thus im using an nucleo board as an debugger , so reset button is pressed in nucleo board, from here via swd connector it will go to mcu respective nrst pin.

so i couldnt able to get why it is happening like this, this first time working in an dual core.

 

 

regards,

srinath

mƎALLEm
Technical Moderator
October 27, 2025

Still not answering all the questions: what is the example are you using for this test?

Did you test the same thing on Nucleo board and it's working?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."