stm32h747xx linker file modifications
Hello everyone!
I have a quick question regarding memory allocation on an STM32H747XIHx MCU. While working with the linker file, I noticed the following memory definitions:
MEMORY {
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K /* Memory is divided. Actual start is 0x08000000 and total length is 2048K */
DTCMRAM (xrw): ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw): ORIGIN = 0x00000000, LENGTH = 64K
}
As you can see, the comment indicates that the total available FLASH memory is 2048 KB, but the linker file only defines 1024 KB.
I then checked the reference manual and found that the FLASH memory spans from 0x08000000 to 0x081FFFFF, which confirms the 2048 KB size. However, when calculating the size using address boundaries (e.g., 0x080FFFFF - 0x08000000), the result is only 2023 KB, not 1024 KB as stated in the linker file. I think this is a misunderstood because I am not taking into account the last address (I should add a +1 when subtracting the boundaries, right?)
A correct approach of a linker file would be:
MEMORY {
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K /* Memory is divided. Actual start is 0x08000000 and total length is 2048K */
FLASH2 (rx) : ORIGIN = 0x08100000, LENGTH = 1024K /* Memory is divided. Actual start is 0x08000000 and total length is 2048K */
DTCMRAM (xrw): ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw): ORIGIN = 0x00000000, LENGTH = 64K
}Additionally, I noticed that the total RAM defined in the linker file is divided as follows:
RAM_D1: 512 KB
DTCMRAM: 128 KB
RAM_D2: 288 KB
RAM_D3: 64 KB
ITCMRAM: 64 KB
The sum of these gives a total RAM size of 1056 KB, not the 1 MB typically mentioned in documentation. Could anyone confirm if this breakdown is correct or if I’m missing something?
Thanks in advance for your help!