Skip to main content
Associate II
March 7, 2026
Solved

STM32H7B3I-EVAL – CubeIDE not opening .ioc; missing MCU package manager

  • March 7, 2026
  • 1 reply
  • 255 views

Hello STMCommunity,

I am a beginner working with the STM32H7B3I-EVAL evaluation board (MCU: STM32H7B3LIH6Q) and I am currently setting up my development environment on Ubuntu 24.04 Linux.

I installed STM32CubeIDE using the following installer:

st-stm32cubeide_2.1.0_27993_20260219_1630_amd64.deb_bundle.sh. zip

However I am facing several issues during setup and project creation.

Problems I am facin

  1. Embedded Software Package Manager missing

    • I cannot find the option: Help → Manage Embedded Software Packages

    • The STM32H7 firmware package does not appear to be installed.

  2. Unable to create a proper project

    • When creating a new STM32 project for STM32H7B3I-EVAL, the project builds incorrectly and sometimes shows: make: *** No rule to make target 'all'. Stop.

    • The expected firmware output files (.elf, .hex, .bin) are not generated.

  3. CubeMX integration problem

    • It appears that STM32CubeMX is not properly integrated with STM32CubeIDE on my Linux system.

  4. .ioc file does not open

    • When I double-click the .ioc file in STM32CubeIDE, the CubeMX configuration window does not open.

  5. Please Provide me Existing Demo Codes:  For this Board also provide Demo Code which is Flashed in Board Firmware version is  V1.0.1 give me correct code. Provide me LED, ADC, Other periphearal Demo codes separately I am using Linux Ubuntu 24.04.3 LTS.
  6. WiFi module issues

    • In  Existing Demo Code  The board includes a WiFi module Available WiFi Show I use correct password but unable to connect wifi , but I am not able to find working demo examples or documentation explaining how to test or use the WiFi functionality on this evaluation board.                                                                                                                                                                                                                         Thank You.

       

       

Best answer by TDK

Use the standalone STM32CubeMX program to create projects. This functionality has been removed starting with STM32CubeIDE v2.0.

STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community

1 reply

TDK
TDKBest answer
Super User
March 7, 2026

Use the standalone STM32CubeMX program to create projects. This functionality has been removed starting with STM32CubeIDE v2.0.

STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
March 9, 2026

 

Hello STMCommunity,

I am a beginner working with the STM32H7B3I-EVAL evaluation board (MCU: STM32H7B3LIH6Q) and I am currently setting up my development environment on Ubuntu 24.04 Linux.

I installed STM32CubeIDE using the following installer:

st-stm32cubeide_1.18.0_24413_20250227_1633_amd64.sh.zip

Problems I am facin

  1. Please Provide me Existing Demo Codes:  For this Board also provide Demo Code which is Flashed in Board Firmware version is  V1.0.1 give me correct code. Provide me LED, ADC, Other periphearal Demo codes separately I am using Linux Ubuntu 24.04.3 LTS.
  2. WiFi module issues

    • In  Existing Demo Code  The board includes a WiFi module Available WiFi Show I use correct password but unable to connect wifi , but I am not able to find working demo examples or documentation explaining how to test or use the WiFi functionality on this evaluation board.                                                                                                                                                                                                                         Thank You.

Andrew Neil
Super User
March 12, 2026

You have a separate thread on that question: STM32H7B3I-EVAL: Need demo codes, Wi-Fi support; Ubuntu 24.04

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.