Skip to main content
Visitor II
February 12, 2026
Question

STM32N6 CoreMark with GCC

  • February 12, 2026
  • 0 replies
  • 365 views

Hello ST Community!

I am currently considering an STM32N6 for a new project and decided to use CoreMark as one of the benchmarks to compare candidates. According to its datasheet and published results on https://www.eembc.org/viewer/?benchmark_seq=13733, the STM32N657 should reach a score of ~3616. I noticed that the published results on the EEMBC website report usage of “ArmClang v15.0 - Keil v6.18” as the compiler. I figured it would be worthwhile checking what score I’d get from STM32CubeIDE’s GCC toolchain.

I ran the test on a NUCLEO-N657X0-Q board and obtained a CoreMark score of 2389, which is quite a bit lower than I expected when comparing against the published results.

The test application is designed as follows:

  • CoreMark source code from https://github.com/eembc/coremark using the instructions in barebones_porting.md.
  • CPU clocked at 800 MHz.
  • Overdrive voltage obtained from external power supply (Pin PB12 = 1).
  • Code runs from ITCM.
  • Data and Stack are placed in DTCM.
  • Interrupts and SysTick timer are disabled during the CoreMark test execution.
  • Optimization set to -Ofast.

I confirmed that my timer (TIM2 configured at 100 MHz) and CPU clock frequency are correct using external equipment and the CM55’s DWT cycle counter.

I also tried:

  • Enabling Link-Time Optimization by adding -flto to compiler and linker options.
  • Leaving the code in the SRAM and enabling cache.

But neither of those gave a better result than the initial configuration.

Are there CoreMark test scores available with ST’s own toolchain that I could compare with?

Is the “ArmClang v15.0 - Keil v6.18” toolchain really that much better than GCC at producing executable object code for the CoreMark test that it explains that large of a gap in test score?

Any additional suggestions on what should be configured to reach maximum performance?

Thanks!