Target No Device Found - Error in Initializing ST-LINK Device
Hello ST Community,
I'm experiencing an issue with my STM32 development setup in STM32CubeIDE. When I try to connect to my target device [ STM32WLE5JC Module(LoRa-E5 mini)] using the ST-LINK, I receive the following error:
"Target no device found, Error in initializing ST-LINK device.
Reason: No device found on target."
My Setup:
----------------------------
IDE: STM32CubeIDE
ST-LINK SN : 260023000B33353739303541
ST-LINK FW : V2J45S7
MCU: STM32WLE5JC(LoRa-E5 mini)
Steps Taken:
----------------------------
- Verified physical connections.
- Powered the microcontroller adequately.
- Used ST-Link utility and CubeIDE for debugging.
- Configured the software environment for SWD.
I'm reaching out to the community for insights into resolving the connectivity issue. If anyone has encountered similar problems or has expertise in debugging STM32 microcontrollers, your input would be highly appreciated.