Skip to main content
Associate III
November 5, 2024
Question

The interface firmware FAILED to reset/halt the target MCU

  • November 5, 2024
  • 1 reply
  • 1241 views

"I'm working with STM32 NUCLEOF429ZI but I encountered this error. Right after I plugged in the cable to upload the program, the txt file showed this error. Please help me identify the cause and how to fix it."

"The interface firmware FAILED to reset/halt the target MCU"

1 reply

Ghofrane GSOURI
Technical Moderator
November 5, 2024

Hello @QuangIoT 

First let me thank you for posting.

 Here are some potential solutions:

Check Connections:
Ensure that all connections between the ST-LINK and the NUCLEO board are secure and correct. Verify that the SWD pins are properly connected.
Reset Procedure:
Hold down the RESET button on the NUCLEO board while clicking the "Connect" button in STM32CubeProgrammer. Release the RESET button once connected.
Power Supply Verification:
Check that your NUCLEO board is powered correctly. Measure the voltage at the power pins to ensure they are receiving sufficient voltage (typically 3.3V).
Use STM32CubeProgrammer:
Connect to the MCU in "Under Reset" mode using STM32CubeProgrammer, which allows you to communicate with the device even if it is in a non-responsive state. Perform a full chip erase if you can connect successfully.
Firmware Update:
Make sure both your ST-LINK firmware and NUCLEO board firmware are up-to-date. You can update ST-LINK firmware using STM32CubeProgrammer.
Isolation from Other Connections:
If your NUCLEO board is connected to other hardware (like breadboards), try isolating it from those connections to prevent interference.
Replace Hardware:
If all else fails, consider that there may be a hardware fault with either your NUCLEO board or its MCU, and replacing it might be necessary.

 

Please check those POST1 and POST2

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.