Toolchain Manager is painfully slow
The Toolchain Manager takes 5–10 minutes to load the toolchain list, even with only a few installed.
It happens every first time I open it after launching the IDE.
If I close it and reopen it during the same session, it loads instantly.
But if I restart the IDE, the delay returns.
Is this normal behavior?
If so, is there anything that can be done to speed it up?
STM32CubeIDE
Version: 1.18.1
Build: 24813_20250409_2138 (UTC)