TouchGFX - generated code - Screen1View
Hello,
I am trying to learn a structure that is provided for MVP implementation. I dont understand where is Screen1View and every other class instance placed. I see that definitions are in .hpp files and implementations of .cpp file. Also, I am really curious where is the Screen1Presenter(Screen1View& v) function called.
#ifndef SCREEN1PRESENTER_HPP
#define SCREEN1PRESENTER_HPP
#include <gui/model/ModelListener.hpp>
#include <mvp/Presenter.hpp>
using namespace touchgfx;
class Screen1View;
class Screen1Presenter : public touchgfx::Presenter, public ModelListener
{
public:
Screen1Presenter(Screen1View& v);
/**
* The activate function is called automatically when this screen is "switched in"
* (ie. made active). Initialization logic can be placed here.
*/
virtual void activate();
/**
* The deactivate function is called automatically when this screen is "switched out"
* (ie. made inactive). Teardown functionality can be placed here.
*/
virtual void deactivate();
virtual ~Screen1Presenter() {};
virtual void setLight (bool state);
private:
Screen1Presenter();
Screen1View& view;
};
#endif // SCREEN1PRESENTER_HPP