Skip to main content
ozzdemir
Associate
August 6, 2019
Question

Unable to use SWV Data Trace Timeline Graph

  • August 6, 2019
  • 4 replies
  • 5646 views

Hello,

I want to use SWV Data Trace Timeline Graph but when I try to open "Configure trace" option, nothing happens, not a single window is being opened etc. Is it some kind of bug, does it have a solution? Thanks in advance.

My IDE and other information are as follows:

STM32CubeIDE

Version: 1.0.2

Build: 3566_20190716-0927 (UTC)

OS: Ubuntu 16.04

Board: Nucleo-F401RE

--

Oguz

4 replies

Markus GIRDLAND
ST Employee
August 7, 2019

Are you in a live debug session when you try to configure the trace or have you just switched to the debug perspective?

Have you activated SWV in the debug configuration?

ozzdemir
ozzdemirAuthor
Associate
August 7, 2019

I was in a live debug session, I was also observing the live expression of the same variable I was trying to plot. I activated SWV in the debug configuration but then "Configure trace" option became deactivated so I reverted it back.

Markus GIRDLAND
ST Employee
August 9, 2019

Does this happen with any project you're creating? Do you have another board to test it on?

I haven't been able to recreate the problem myself but I'll give it a try on the Linux computer to see if it's OS specific later today.

ozzdemir
ozzdemirAuthor
Associate
August 9, 2019

Yesterday, I tried again to activate SWV and was able to open the window and configure this time, I don't know what changed from then.

Thanks for your effort.

benjaminu
Visitor II
October 7, 2023

It is not OS-dependent. In any case at least some feedback to the user is required even if these settings require an active debug session.

Bitschubse
Associate II
February 22, 2024

Hi,

is there any solution to this problem?

I tried to configure the trace in every SWV View. But the window does not open. It doesn't matter if I am in an running debug session, a halted session or if I just opened the debug perspective. There is no reaction if I click on this icon.

Please help.

Best regards

Alex

 

Visitor II
December 13, 2024

After a lot of struggling, I figured it out that you need to hit the down arrow of debug button (bug), debug configuration, debugger and ENABLE SWV checkbox!!!!! It solved the issue for me!

rbclima_0-1734054469560.png