Skip to main content
Associate III
October 29, 2024
Question

Why stmcubeIDE don't import my projects correctly?

  • October 29, 2024
  • 1 reply
  • 902 views

I have an issue here with the IDE. i have few projects compressed in .rar that I am using since the start of the year and everything worked well until this week. When i try to import one of these projects (any project) to my IDE, it shows me this window:

Captura de pantalla 2024-10-29 122600.jpg

And it always showed something like "Import Successfully"...

I am using version 1.16.1 and i tried to downgrade to 1.14.0 because in other computer with this version still works.

I have checked the .cproject and .project files but everything seems well... I am 99% sure that is anything about the IDE.

 Why it is happenning to me? How can i solve this issue?

Thank you so much.

1 reply

Technical Moderator
October 31, 2024

Hello @rubenles ,

Are you using the "Copy into workspace" option ?

Maybe you have this known issue:

68184 Hierarchical projects cannot be imported with the option Copy into workspace.

listed in the STM32CubeIDE:STM32CubeIDE errata 1.16.x - stm32mcu

 

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
rubenlesAuthor
Associate III
November 4, 2024

Hi Imen.D.

I am openning the project by double clicking on the .cproject file and then, the window i add before appears. It has no option to show any issue... I can't import this project basically.

Thank you for answering.