Skip to main content
SRedd.5
Senior III
September 27, 2023
Solved

CubeMonitor frequently Disconnects

  • September 27, 2023
  • 4 replies
  • 2754 views

The cube monitor frequently disconnects while capturing data. How do i solve this problem i want to log data continuously. The other problem is when i am saving the data as below

SRedd5_0-1695829037054.png

i do not know the location where the csv file is stored. Please help.

    This topic has been closed for replies.
    Best answer by Richard.Chvr

    Did you have a look to this topic

    4 replies

    Richard.Chvr
    Technical Moderator
    September 28, 2023

    Hello @SRedd.5 

    The directory path where you can find the log files could be configured in settings.js file ( default path is home directory / log ).

    For the disconnection issue, which STM32 device is attached to the cubeMonitor?

     

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    SRedd.5
    SRedd.5Author
    Senior III
    September 28, 2023

    The directory path where you can find the log files could be configured in settings.js file ( default path is home directory / log ).

    When you say settings.js is the below file

    SRedd5_0-1695909260322.png

    what changes i need to do to change the log path.

    I have already have several .stcm files i want to convert to csv files. when i read the ST community i came across the below i have added as attachment

    But i am not able to convert, do i need to have the tool connected or can it be done offline 

    For the disconnection issue, which STM32 device is attached to the cubeMonitor?

    SRedd5_1-1695909611950.png

    The above tool and the cubemonitor detects the below

    SRedd5_2-1695909680192.png

    It will really help me if the tool does not disconnect then i can watch the data clearly.

    Richard.Chvr
    Technical Moderator
    September 28, 2023

    Please have a look to stm32cubeMonitor wikis:

    https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:How_to_change_general_settings

    https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:How_to_log_data_in_a_.csv_file 

    I can see you've attached a STLinkV2 but what is the device probe connected to the STLINK?

     

     

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    SRedd.5
    SRedd.5Author
    Senior III
    September 28, 2023

    I really don't understand the device probe mean, but the below is the configuration i use when connecting the ST link debugger when running Cube Ide. Is this what you are asking?

    SRedd5_0-1695915492333.png

     

    Richard.Chvr
    Technical Moderator
    September 28, 2023

    Just wanted to know which MCU you're using,  STM32xxxxx? Because some devices like STM32WB55xx goes to sleep mode to optimize power consumption and therefore disconnects. 

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    SRedd.5
    SRedd.5Author
    Senior III
    September 28, 2023

    STM32G431RBTX is the micro and it is motor control application, when i give command to start the motor then it gets disconnected it is just one observation not every time. 

    Richard.Chvr
    Richard.ChvrBest answer
    Technical Moderator
    October 5, 2023

    Did you have a look to this topic

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.