Loading ELF in STM32CubeMonitor stuck at 25% in Ubuntu 18.04
I have just installed STM32CubeMonitor as an alternative to STM32Studio since I am no longer using Windows. I have been a happy user of STM32Studio but have been frustrated with the lack of Linux support, so I was excited to see that STM32CubeMonitor supported Linux.
Unfortunately my first experience with it did not meet my expectations.
- I have not been able to load an ELF file since the ELF parser gets stuck at 25% (see the attached picture)
- After manually entering the addresses I was able to view the data but only at a slow sample/refresh rate of what appears to be 10 Hz or less. I tried to modify the Sampling Frequency in the Variables node but this did not seem to have any effect.
Finally I would also like to ask about why both the Probe Out and Probe In is needed when you only want to do acquisition (input). Why is the Probe Out needed?
Best regards
Thomas Jespersen