Probe reports 0 for all monitored variables
On a custom STM32H523-based board connected via STLink 2.0 (swd, p2p in CubeMonitor), all selected variables are plotted as 0, including those whose initial value is not 0. I used the Basic_Flow template, where I set acq_out, acq_in, and loaded variable addresses from an ELF following this guide. The executable is proven to update values under GDB. I have tried rebuilding with -O0 and reconnecting and changing sampling frequency between sequential loop and 10 Hz. The code does not contain any standby instructions and the port looks fine since GDB works. I would appreciate any help or advice.