Skip to main content
Kmax18
Senior II
September 1, 2025
Solved

STM32CubeMonitor shows erroneous zero values in time series

  • September 1, 2025
  • 1 reply
  • 354 views

Hello, I am using the STM32CubeMonitor software for the first time and find it very helpful. My question is about the root cause for erroneous zero values in the time series displayed by the STM32CubeMonitor software. It's first first use was monitoring the joystick x/y displacement signals of the Adafruit Gamepad QT. 

Question: What is the root cause for the phenomenon of erroneous zero values? Are parameters in my Basic Flow configuration incorrect? (Note: the zero values are not consistently present in the graphs, sometimes the signals are 'clean'.)

Question: where are the Monitor Flow files saved on disc (Windows 11).

Technical details:

  • Figure 1 shows the test setup with the Gamepad and the Nucleo-G071RB board. Pairs of 16-bit data points were received by the Nucleo board using the I2C protocol (hi2c1). I confirmed that the x/y signal integrity was good: no outliers or erroneous values were received by the Nucleo board, the I2C master.
  • Figure 2 shows a Basic Flow used with the STM32CubeMonitor software for monitoring the x/y time series.
  • Figure 3 shows the Node-RED Dashboard with the constant value (490) of the joysticks x-axis. The graph also show regular zero values, which are not present in the original time series received by the Nucleo board.
  • Figure 4 shows the same time series as Figure 3, but zoomed in on three groups of zero values.

Figure 1. Test setup with Gamepad QT and Nucleo board.

Kmax18_3-1756699527706.png

Figure 2. STM32CubeMonitor Basic Flow.

Kmax18_0-1756699165858.png

Figure 3. STM32CubeMonitor Node-RED Dashboard.

Kmax18_1-1756699363624.png

Figure 4. Node-RED Dashboard, zooming in on zero value groups.

Kmax18_2-1756699422477.png

 

    Best answer by Kmax18

    Update: this issue has not re-occurred in 24 hours, so I assume that the described behavior was an outlier. I must somehow fixed the issue. Case closed...
    Thanks for reading this. Have a great day!

    1 reply

    Kmax18
    Kmax18AuthorBest answer
    Senior II
    September 2, 2025

    Update: this issue has not re-occurred in 24 hours, so I assume that the described behavior was an outlier. I must somehow fixed the issue. Case closed...
    Thanks for reading this. Have a great day!