Skip to main content
Visitor II
June 22, 2023
Question

STM32CubeMonitor stuck at 10% when parsing .elf

  • June 22, 2023
  • 1 reply
  • 828 views

When compiling with Maximum (-g3) Debug level, Add new exe-config config mode stalls at 10% when loading .elf. Why is this? Is there a limit to the number of symbols or the size of the .elf?

If compiled with Default (-g) Debug level, then loads OK.

When the project was simpler, fewer files, it did load OK with-g3 Debug level.

STM32 CubeMonitor version 1.6.0     Windows 11
GNU Tools for STM32 (10.3-2021.10)

    This topic has been closed for replies.

    1 reply

    Richard.Chvr
    Technical Moderator
    August 31, 2023

    Hello @_kj_ 

    What is the size of your elf file? Can you share it?

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.