Skip to main content
paolog
Associate III
January 12, 2024
Solved

X-NUCLEO-LPM01A installation issue

  • January 12, 2024
  • 1 reply
  • 1093 views

Hi!

I'm having problem connecting the board to a Windows 10 PC. Connecting the board to the USB it works in standalone mode, but the USB driver (PowerShield Virtual ComPort in FS Mode) is not installed, so I can't use the board with the STM32CubeMonitor-Power. Windows Device Manages tells that device drivers have not been installed, and the associated COM port is obviously not existing.

Is the X-NUCLEO-LPM01A not functioning properly or am I missing something?

    This topic has been closed for replies.
    Best answer by paolog

    Ok, I just needed to upgrade the firmware of the X-NUCLEO-LPM01A...

    1 reply

    paolog
    paologAuthorBest answer
    Associate III
    January 13, 2024

    Ok, I just needed to upgrade the firmware of the X-NUCLEO-LPM01A...