STM32CubeMX2 + NUCLEO-C562RE - you need AI?
Finally was able to test STM32CubeMX2 with a NUCLEO-C562RE board.
Simple LED blinking project, and here's what I found out.
Project bloat:
STM32CubeMX2: 26.2 MB of generated data and when compiled 41.1 MB (NUCLEO-C562RE)
STM32CubeMX: 4.6 MB generated and compiled 15.7 MB (NUCLEO-C031C6, same functionality)
The old STM32CubeMX included only the HAL libraries actually used.
The new one dumps everything in.
That's a 5.7x increase for a blink LED.
Missing Release configuration:
Generated CMake project contains only Debug configuration - No Release.
Interesting, because the official "MOOC STM32CubeMX2" video at 4:53 clearly shows both configurations.
Either something changed or the video is misleading.
Creating Release configuration manually requires editing multiple CMake files, including inside the cmake folder — supposedly overwritten on regeneration (in practice, changed only at project creation).
Not trivial if you're not a CMake expert.
I did it once manually, but then ended up using Claude Code AI to do it quickly again.
Linker files buried deep:
The .ld linker files are now hidden under several directory layers (previously at project root).
If you need separate linker configurations for Debug and Release — different memory layouts, for instance — good luck doing that without solid CMake knowledge.
Again, I had to ask AI for help. It's doable, but shouldn't be this complicated.
Bottom line:
The tools work.
If you don't have some CMake experience, will add extra friction.
But basic tasks like Release builds and linker customization shouldn't require AI assistance.
The new interface is fine, just needs getting used to — many settings have moved around.
But a designer tool should better handle these common workflows, not make them this complicated.
Suggestions:
Generate both Debug and Release configurations by default
Include only required HAL driver files
Make linker file customization more accessible