Skip to main content
MSSloan1962
Associate III
September 29, 2022
Question

Are there examples of STM32CubeProgrammer API usage within C# applications

  • September 29, 2022
  • 0 replies
  • 714 views

I am trying to create a C# application within Visual Studio 2019 for using STM32CubeProgrammer API because I will need to modify an existing C# application to use it. At the moment I am having trouble connecting to the small board I am using:

      int connectionResult = CubeProgrammerApi.Connect(cbUsbIndexes.SelectedItem.ToString());

      CubeProgrammerApi.Disconnect();

With both of these routines I am getting 0xC0000005: Access violation executing location 0x0000000000000000 errors.

I do seem to have gotten the getDfuDeviceList working:

      _deviceInfo = AddressOf(ref _dfuDeviceInfo);

      _numberOfDfUDevices = CubeProgrammerApi.GetDfuDeviceList(ref _deviceInfo);

The DLL Imports I have defined are as follows:

    [DllImport(DllPath, EntryPoint = "getDfuDeviceList", CallingConvention = CallingConvention.Cdecl, CharSet = CharSet.Ansi)]

    internal static extern int GetDfuDeviceList(ref IntPtr dfuDeviceInfo, int intPid = 0xdf11, int intVid = 0x0483);

    [DllImport(DllPath, EntryPoint = "connectDfuBootloader", CallingConvention = CallingConvention.Cdecl, CharSet = CharSet.Ansi)]

    internal static extern int Connect(string usbIndex);

    [DllImport(DllPath, EntryPoint = "disconnect", CallingConvention = CallingConvention.Cdecl, CharSet = CharSet.Ansi)]

    internal static extern void Disconnect();

    [DllImport(DllPath, EntryPoint = "deleteInterfaceList", CallingConvention = CallingConvention.Cdecl, CharSet = CharSet.Ansi)]

    internal static extern void DeleteInterfaceList();

This topic has been closed for replies.