Cannot connect to target if there is another ST-Link connected
I'm working in an environment with multiple targets and ST-Links.
In previous versions of CubeProgrammer I had no problem to connect to a target with serial number X while other targets that are connected with other ST-Link are connect to the debugger (CubeIDE)
After I start to work with 2.8 I get ST-LINK error (DEV_CONNECT_ERR) when I try to connect to target X while other targets are connected to the debugger.
Only if I stop the debugger on all others ST-Links the programmer connect successfully.
Any idea?