Skip to main content
TDJ
Senior III
April 5, 2024
Question

CubeProgrammer 2.16 CLI problem - warning

  • April 5, 2024
  • 1 reply
  • 844 views

After upgrading CubeProgrammer to new release 2.16 CLI commands started to fail during verification phase when changing option bytes on STM32U5A5. Sample command which fails:

STM32_Programmer_CLI -c port=SWD mode=UR --hardRst -ob WRP1A_PSTRT=0xff WRP1A_PEND=0

The same operation performed from GUI works correctly. I had to go back to release 2.15

This topic has been closed for replies.

1 reply

STTwo-32
Technical Moderator
April 5, 2024

Hello @TDJ 

I've tested using the NUCLEO-U5AZJ-Q:

STTwo32_0-1712308071982.png

The default value of the WRP1A_PSTRT and WRP1A_PEND are 0xFF and 0x0:

STTwo32_1-1712308209835.png

Then, using the command " STM32_Programmer_CLI -c port=SWD mode=UR --hardRst -ob WRP1A_PSTRT=0xaf WRP1A_PEND=1 ",I've been able to set the WRP1A_PSTRT and the WRP1A_PEND to 0xAF and 0x1:

STTwo32_2-1712308476181.png

and Finally I've executed the command " STM32_Programmer_CLI -c port=SWD mode=UR --hardRst -ob WRP1A_PSTRT=0xff WRP1A_PEND=0 " which take back the WRP1A_PSTRT and the WRP1A_PEND to 0xFF and 0x0:

STTwo32_3-1712308813082.png

Can you add more details about your issue (screenshot,...).

Best Regards.

STTwo-32