Skip to main content
KFang.1
Associate II
April 24, 2020
Question

CubeProgrammer connect to UART interface

  • April 24, 2020
  • 5 replies
  • 14955 views

I am using CubProgrammer (version 2.4.0) to update the flash on NUCLEO-G070 board.

When I select the device target i/f as ST-Link and connect, I can do flash programming.

When I select the target i/f is UART, the Com Port shows up correctly about this device. However, I couldn’t connect. The error message is:

Serial Port COM4 is successfully opened.

17:48:09 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off

17:48:10 : Timeout error occured while waiting for acknowledgement.

17:48:10 : Timeout error occured while waiting for acknowledgement.

Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

Do I need to put the STM32G07 Boot0 pin LOW? What am I missing? 

Another question:

Is the Flasher-STM32 a subset of the CubProgrammer? It can only do flash programming with target device i/f is UART? 

This topic has been closed for replies.

5 replies

TDK
Super User
April 24, 2020

If you want to use the UART bootloader to connect to the board, you need to put the MCU in bootloader by holding BOOT0 during reset.

"If you feel a post has answered your question, please click ""Accept as Solution""."
RShar.8
Associate
May 23, 2022

Thanks dear,

I was frustrated for last 4 days as was not able to programme but your this small instruction solved my problem- Thanks a lot

Houda GHABRI
ST Employee
May 3, 2020

Hi @KFang.1​ 

in order to use UART interface for Firmware download you have to check you are booting on System bootloader.

To force boot on system bootloader (instead of User Flash) you can set this Option Byte configuration (using STLink Interface with STM32CubeProgrammer) :

nBOOT_SEL => Checked.

nBOOT1 => Checked.

nBOOT0 => Unchecked.

best regards,

Houda

KFang.1
KFang.1Author
Associate II
May 14, 2020

Thanks. This works! I had another follow up question with that. I'll submit as a new case.

What happen is that I didn't Unchecked the nBOOT0 (and nBOOT_SEL is check), now after I programmed the device once successfully, I can no longer put the device in bootLoader mode (pull the bootmode pin high during reset would not help). How to recover that? Where and how to modify the bootloader configuration setting?

TDK
Super User
May 14, 2020

You can change the option bits (nBOOT0, nBOOT_SEL, etc.) using ST-Link. If you disabled the system bootloader, that's your only option.

"If you feel a post has answered your question, please click ""Accept as Solution""."
KFang.1
KFang.1Author
Associate II
May 14, 2020

Thanks for the fast reply! I can use the ST_Link to connect it and have the nBOOT_SEL uncheck (back to legacy mode) and click "apply". Now I can flash in a new program. However, I still can not put the device in BootLoader mode by using the BootMode pin (hold BootMode pin high, then press Reset).

MWon.1
Associate
June 15, 2021

Hi,

I'm having the same problem and I can't use your solution.

When I connect STLink I don't have those options in Option Byte menu. I only have BOR_LEV value to define.

I'm working with STM32F411CEU6

TDK
Super User
June 15, 2021

Make a new post will all relevant details rather than jumping on an old one. The STM32F4 doesn't have the same option bytes as the STM32G0.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MWon.1
Associate
June 15, 2021

Ok, sorry... I didn't create a new post because I have exactly the same problem as the initial post (can't interface with UART).

I just follow the general rule to not open a new thread if the root problem seem to be the same.