CubeProgrammer won't work properly
After updating and restarting my PC with Windows 10, my old version of CubeProgrammer would not open at all. The version number is unknown. Other STM32 software works without any issue such as CubeMX and CubeIDE.
I then tried installing the latest version, 2.21.0. The program launched (even when run as administrator), but it did not function fully. I attached a screenshot for reference. None of the four icons on the top-left responded, and I received error messages when clicking the icons on the right.
I also tried installing previous versions from 2.16.0 to 2.20.0, but none of them worked. Specifically:
Versions 2.16.0, 2.18.0, and 2.19.0 briefly showed the launch logo, then closed immediately.
Versions 2.20.0 and 2.21.0 would open, but the program remained unusable.