DFU mode read out protection
Hello,
I am trying to connect to the STM32F072C8T6 microcontroller via USB in the STM32CubeProgrammer, however I am getting:
"Device is under read out protection ! If you want to disable RDP please reconnect with Read Unprotect enabled"

So, when I check the Read Unprotect (MCU) checkbox, I get:
"Please Power off Power on your device."

After turning the power off/on, I see the same messages. I cannot connect to the MCU via USB in the STM32CubeProgrammer.
I have tried different versions of STM32CubeProgrammer:
- v2.16.0
- v2.15.0
- v.2.13.0
- v.2.10.0
- v.2.8.0
Moreover I tried on second computer with Windows 11 and I have the same issue.
I'm trying to connect my custom board, but I also checked another hardware board (BluePill ) with the same STM32F072C8T6 MCU and it doesn't work either.
Interestingly, using the DFU-util v0.8 program I can connect to the MCU and successfully read/write memory: