"Error: Database: There's no active configuration for this device"
I have a STM32H730 device, with a STLINKV3-SET connected via SWD (3 pins).
When I Connect using STM32CubeProgrammer I get the following popup message;
Error: Database: There's no active configuration for this device. All the 4 configurations are disabled!
However the Connection appears to be okay, I can read/modify the SRAM memory and erase the Flash.
So what does this error mean?
Does is need to be addressed?
I have updated STM32CubeProgrammer and the STLINKV3-SET firmware to latest.
Thank you.