[Feature request] Pass binary key to wusrkey instead of file path
Currently, the STM32CubeProgrammer CLI allows loading keys into the second CPU of an STM32WB using the wusrkey command. For example, we use it in combination with SBSFU. This command currently requires a path to a file containing the binary key.
My request /propousal would be for this command (or a new one) to also accept the binary key directly (instead of a path to the key file). This way, in flashing tools used in production that need to write this key running this command, there would be no need for a file on the file system, and they could directly provide the key stored in memory (which can be retrieved from a secret management service). This would enhance the security of key custody (enhance, not eliminate, as that is impossible).