Skip to main content
OMarc.1
Associate II
February 6, 2020
Question

Flash Loader in Nucleo-STM32F401 (Unrecognized device)

  • February 6, 2020
  • 2 replies
  • 777 views

Hi everyone.

I have a board Nucleo-STM32F401, and i will try to write the program on STM32f401 with RS-232 communication, i did like in pdf, BOOT0 with jumper connect to Vcc (CN7 5pin+7pin) and i have the simple device RS232 to USB, and RX/TX connect to PA9/PA10 (CN10 33 and 21 pins), and of course GND pin to GND of RS-232.

Power supply i take from USB, the board always connects with USB-mini to PC.

And when i try to use Flash Loader i have a message:

Unrecognized device.. Please, reset your device then try again.

(I tried).

Parameters of Flash Loader like in pdf.:

Baud rate 115200;

Prity Even;

Echo Disabled.

When i tried to use STM32CubeProgrammer, 

And i have another error:

Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

Can you help me? It's my first experience with STM controllers, maybe i need to do something to turn it on? Maybe i should write the program, and write program to the controller, and after that, i will have a possibility to use RS-232 programming? 

This topic has been closed for replies.

2 replies

Technical Moderator
February 6, 2020

Which STM32CubeProgrammer version are you using ?

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
OMarc.1
OMarc.1Author
Associate II
February 6, 2020

Last version from the site 2.3.0