G474RE single bank configuration not correctly shown by STM32CubeProgrammer in DFU USB mode
STM32G474RE flash in single bank configuration is not correctly managed with STMCubeProgrammer if connected to target in DFU USB mode. In that configuration always 256 pages of 2K size are shown. If I connect STM32CubeProgrammer via ST-LINK to the same target then 128 pages of 4K size are correctly shown. Is there any reason? Is it a known bug?