Getting Started Guide - CubeProgrammer GUI not working but CLI works just fine.
I just installed the CubeProgrammer and I'm following the Populate the target and boot the image guide. When I get to section 1.1.1.1.2.6 Populate the SDCard and click "Connect" I get this error:
But if I execute this on the command line:
sudo /opt/st/stm32cubeprgrammer_2.9.0/bin/STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsvEverything works perfectly fine. I get this:
Is anyone familiar with that error on the GUI? If it works on the CLI it should work on the GUI too, isn't it?