Help connecting to STM32 on Cube Programmer
Hello everyone,
I have a PCB with an embedded STM32F103 on it. The PCB provides access to some ports on the side. Those are linked to VDD, PA9, PA10, PA13, PA14 and GND.
I tried connecting to it with Cube Programmer using a FT232RL as pictured below :
The connections are :
3.3 v -- VDD
GND -- GND
RX -- PA10
TX -- PA9
When I try to connect with Cube Programmer it shows an error :
I tried all baud rates as I have no idea which one I should use but still no luck.
On the PCB it looks like pin boot 0 is connected to a resistance which is connected straight to ground and same for pin PB2.
Any idea on what I am doing wrong ? (I'm fairly new to this so it might be a stupid mistake)
Thanks in advance !