Hi, I'm attempting to read memory data of my STM32F030c8t6_board (I got boards on banggood.com, picture in details section). I can not connect to my device. See details section for explanations. Best regards, Sylvain
Used tools:
- stm32cubeprogrammer
- STLink-v2 (wired pins: 7:swdio, 9: swclk, 1: vcc, 8: gnd), the dev board usb is plugged to supply the chip.
- tried with all reset combinations, bus clock configs and boot0 config.
- tried with openocd as well (see console log below)
- tried with one of my own board (stm32f4x) to check if my tools are still working properly, I can read memory of the chip perfectly.
Questions:
- Do I miss something to make chip debug probe connection working ? I generally never had trouble to connect it to my boards. Anyway this is the first time I work on STM32f0 series.
- I heard possible fake MCU's sold on some websites (I used banggood, the price were quite low), do you thing it could be the case ?
Log of stm32cubeprogrammer:
16:12:13 : ST-LINK SN : 55FF6F064986565728531287
16:12:13 : ST-LINK FW : V2J37S7
16:12:13 : Board : --
16:12:13 : Voltage : 3.28V
16:12:13 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)
16:12:18 : ST-LINK SN : 55FF6F064986565728531287
16:12:18 : ST-LINK FW : V2J37S7
16:12:18 : Board : --
16:12:18 : Voltage : 3.28V
16:12:18 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)
16:12:23 : ST-LINK SN : 55FF6F064986565728531287
16:12:23 : ST-LINK FW : V2J37S7
16:12:23 : Board : --
16:12:23 : Voltage : 3.28V
16:12:23 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)
16:12:35 : ST-LINK SN : 55FF6F064986565728531287
16:12:35 : ST-LINK FW : V2J37S7
16:12:35 : Board : --
16:12:35 : Voltage : 3.28V
16:12:35 : Error: No STM32 target found!
Log from openocd:
openocd -f /usr/share/openocd/scripts/interface/stlink-v2.cfg -f /usr/share/openocd/scripts/target/stm32f0x.cfg -c 'init'
Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 1000 kHz
adapter_nsrst_delay: 100
none separate
Info : Unable to match requested speed 1000 kHz, using 950 kHz
Info : Unable to match requested speed 1000 kHz, using 950 kHz
Info : clock speed 950 kHz
Info : STLINK v2 JTAG v37 API v2 SWIM v7 VID 0x0483 PID 0x3748
Info : using stlink api v2
Info : Target voltage: 3.282795
Error: init mode failed (unable to connect to the target)
in procedure 'init'
in procedure 'ocd_bouncer'