Skip to main content
DK.7
Associate III
July 11, 2022
Solved

How do i need to create .bin file for an QSPI memory?

  • July 11, 2022
  • 1 reply
  • 2217 views

I am a beginner and I do according to this video "External Qaspi Loader How to - 05 - Qspi Driver Coding" https://youtu.be/XqCq0xtQmbI I uploaded the project "EXTERNAL QSPI Loader" to stm and now question about .bin file

How to create a data file to be stored in the Flash memory,

which can be a binary file or .hex?

For example, I have a project "Hello World" and I want to upload it to external QSPI memory.

I need as usual to create a project "Hello world" and just indicate in the stm32CubeIDE settings to create a .bin

Or I need to make some additional settings for my "Hello world" project like, MPU configuration!?!

And the resulting file, to program Quad-SPI Flash memory using the ST-LINK utility...

This topic has been closed for replies.
Best answer by Tesla DeLorean

From the application side I would avoid reseting or touching the RCC for the most part. Specifically you really don't want to be tearing down the clock sources, PLLs, or reconfiguring or touching anything related to the QSPI.

For example not DeInit'ing the GPIO bank(s)

Contractually you want ALL the system bring-up on the Boot Loader side, ie the clocks the PLL, the system critical pins, etc. The things you will use all the time, and would facilitate system updates and recovery.

You don't have to bring up UART, SPI, I2C that the loader doesn't use. And generally you don't want a lot of interrupts, as these will complicate the hand-over.

The SystemInit() on the App side needs to be relatively lean, perhaps enable the FPU, and assign the new operational SCB->VTOR

1 reply

Tesla DeLorean
Guru
July 11, 2022

STM32 Cube Programmer can take .BIN, .HEX files as input

.BIN files can be created via tools like objcopy, fromelf or srecords

The External Loader files with the .STLDR extension are .ELF files that basically load like DLL files into the STM32's RAM providing support for your hardware, pin, wiring and chip combos.

To run code out of the QSPI memory you'd need some Internal Flash based code to bring up the QSPI memory and transfer control to code in there. This can be part of the app, or as a loader that calls an app that resides completely in the QSPI memory.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
DK.7
DK.7Author
Associate III
July 11, 2022

Thanks for the answer!

I have a board from "Weactstudio" https://aliexpress.ru/item/1005001475058305.html

And they posted on Github an example "02-extm_boot" https://github.com/WeActStudio/MiniSTM32H7xx/tree/master/SDK/HAL/STM32H750/02-ExtMem_Boot

which run the program on 8Mb qspi flash, this routine is QSPI Bootloader, App Addr:0x90000000

For understanding how it works, I tried to upload a simple "Blink" on external QSPI flash...

I uploaded a code "02-extmem_boot" to the internal Flash memory which start from 0x0800000

And also uploaded the "Blink" with "STM32CubeProgrammer" to fed to him the .bin file which uploaded from address 0x90000000.

But it dosn't work!

Could you tell me what I'm doing wrong?

Tesla DeLorean
Guru
July 11, 2022

>>Could you tell me what I'm doing wrong?

Hard to say, use a debugger, step into the loader code, and then thru the transition to your application code.

Make sure the vector table on the "External Blink" at does reflect the 0x90000000 basis, and that the SCB->VTOR settings in SystemInit() do actually set the address to the same 0x90000000 address.

Review the .MAP and .LST (listing/disassembly) of the "External Blink" are consistent with expectations for an image built to execute from QSPI

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..