How to add .obj and .bin (Video file) to external flash memory? (NOR Flash)
Hi Community,
In my project I have successfully added the image buffer in external flash memory and able to read/write to the same. But now I am facing the problem when I added the .obj or .bin videos file in the external flash memory with the help of linker script and STM32CubeProgrammer, but that amount of .obj or .bin file is not appearing in the external memory.
Can You guide me how to add the .obj or .bin video files in External Flash Memory? Is this possible by project code itself or need the edit in the linker script. if yes then pls give me some examples or demo?
/Mit