Skip to main content
Associate
January 12, 2026
Solved

HSM reader detection

  • January 12, 2026
  • 1 reply
  • 312 views

Hi, using STM32 Cube Programmer and STM32 Trusted Package Creator W2.21, I was unable to detect the HSM card, getting error 0x88000002. I had to downgrade to V2.14, as mentionned in several posts to get it detected successfully.

I use HID Omnikey 3121 reader.

Any solution to be able to use last version 2.21 and HSM card ?

Best answer by Aziz BRIGUI

Hi @PLencou,

I can't reproduce the behavior you're seeing, but I don't have the exact reader you're using on hand. According to the last comment on this thread, installing STM32CubeProgrammer to a different path resolved the issue for v2.16. Could you try that and get back to me? Also, can you detect the HSM in STM32CubeProgrammer here ?

AzizBRIGUI_0-1768234531751.png

Aziz

1 reply

Aziz BRIGUI
Aziz BRIGUIBest answer
Technical Moderator
January 12, 2026

Hi @PLencou,

I can't reproduce the behavior you're seeing, but I don't have the exact reader you're using on hand. According to the last comment on this thread, installing STM32CubeProgrammer to a different path resolved the issue for v2.16. Could you try that and get back to me? Also, can you detect the HSM in STM32CubeProgrammer here ?

AzizBRIGUI_0-1768234531751.png

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PLencouAuthor
Associate
January 14, 2026

I confirm it works after I did the installation of the latest version V2.21 on a different folder. Note: I haven't uninstalled the previous version 2.14. Then both version could detect the HSM card and I could program the HSM card successfully.

PLencou_0-1768378666164.png

Thank you for your valuable support.